Motor_L
| Index.Sub | 2005.7H |
| Data Type | Unsigned32 |
| Access | Read/Write |
| PDO Mappable | No |
| Unit | H x10-6 |
|
Range |
Unsigned32 |
| Default Value | 2420 |
| Store Supported | Yes |
| Description |
This object sets the motor L (inductance) used for Motor Current Regulation. This value is used when Motor R,L detection function is disabled (bit#9 of Drive_Working_Settings_Extended object equal to 0). The Nominal_Current of the Motor must be defined. |
|
Notes |
See Motor R, L Detection. |